Part Number: TMS320F28035
Hi Everyone,
I am working on a project to run ac induction motor with ti dsp tms320f28035 using foc.
My motor has rated speed of 3000rpm and max speed of 6000rpm.
I am able to run motor at 3000rpm by giving maximum vq. I used 48V battery pack for this.
My goal is to run motor at 6000 rpm , I am planning to use a 72V battery pack to do so. Can I achieve higher speeds using 72V battery pack , without doing field weakening im the code?