Part Number: TMS320F28388D
Hi,
I have some printf statements in an RTOS based application targeted for F2838x. While I am able to see printf output before starting the scheduler the RTS library based printf present in task functions dont work due to the task stack being around 256 words. I want to use printf_stdarg.c in the project which claims to have stack light versions for the stdio functions. It has an external dependency on putchar() implementation. Is there a way to use RTS library based putchar for the same? I tried using the same but do not see any output on the console. Let me know if this can be done. Please suggest if there are any other alternatives for printing the data for C28x devices with the above mentioned task stack size limitation. Here is the link for the printf_stdarg.c file which I am using for reference.
Thanks
Vasudha