Part Number: TMS320F28388D
Per related documentation (Secure BOOT on C2000 Device, SPRACT3 – SEPTEMBER 2020) is the additional time taken to authenticate first 16KB of flash boot code for CPU1 about 400 ms (Running on INTOSC at 10 MHz).
Is there any option to significantly reduce the 400ms of the secure boot time? For example by increasing the clock to 200MHz, so we could get close to 20ms?