Part Number: TMDSHVMTRPFCKIT

What is the meaning of this warning? Is there any software that i have not installed yet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSHVMTRPFCKIT

What is the meaning of this warning? Is there any software that i have not installed yet?
Older projects when run on latest CCS/compiler may generate this warning. Most times the project should work fine.
Not needed.....If you are interested to know more about CCS, Please go through the materials available on ti.com
https://www.ti.com/tool/CCSTUDIO#support-training
Can you explain what is that you are trying to develop with the KIT?
Oky firstly, this is my final year project for my degree. My final year project is to control the 3-phase motor induction motor (0.75kW) . So my supervisor ask me to use the KIT. So, i want to use scalar V/F Control method.
What i have right now is.
Hardware
-0.75 kW 3-phase induction motor.
-TMDSHVMTRPFCKIT.
-Piccolo F28035 Control Card.
Software installed
-Code Composer Studio v10 ( i have tried v5, v6 and v8) ; all of it stuck at the same step. ( which is all the error that i asked you before).
-Controlsuite
The kits i borrowed from the lab comes with a usb drive which contains.
In the docs file contains

Could you guide me how to complete my project using this kit? Im really appreciate it. It is really important for me. Thank you.