Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG, LAUNCHXL-F28379D,
Hi everybody ,
I m using latest C2000ware and latest CCS .
now using GPIO_EX2_Toggle : used as default it works no problem ( I can change GPIO etc )
now I switch HW to LP -F280049C and if I compile and use a pin for example GPIO 28 it works , but I m not able to use GPIO23 /LED4 ( same issue on LED5 )
no matter if I use the GPIO pin or if I set "use HW " : I always get erros in compiling .
please which is correct way to force Sysconfig to use LED4 in launchpad ?
thank you
BR
Carlo