Part Number: TMS320F28065
Other Parts Discussed in Thread: C2000WARE
Hello,
I am currently designing a small ECU with TMS320F28065 processor. I have few doubts regarding XDS110 debug probe connections as below
1. I am planning to put a small header on my development ECU for connecting XDS110 probe. When I studied the datasheets of processor and XDS probe then I found two pictures as below



First two picture is snapshot from processor datasheet where it is seen that 14 pins are connected. Whereas in third picture (taken from XDS110 probe manual) it is seen that 20 pin connection is used for debug.
I am bit confused if it is just 14 pins of second connector that needs to be populated on my development ECU? And leave remaining pins unconnected?
If above is not the case then what is to be connected to pins 15 to pin 20?
Update: the schematic in ECU for debug connection is as below:

Please suggest on this.