Part Number: TMDSDOCK28379D
Other Parts Discussed in Thread: C2000WARE
Hi Team,
Could you help our customer please. Here is their concern below.
I have a software related question for the TMDSDOCK28379D.
I'm wondering if there is any code available for these controllers that I could use to generate an ePWM signal that will synchronize the ePWM of a second controller.
That way both controllers are producing ePWM signals on roughly the same clock cycles.
I'd like one controller to generate an ePWM that can be used to synchronize a secondary controller's ePWM signals. In other words, I'd like both controllers to generate multiple ePWM signals that occur with little time delay between them, and I understand this synchronization must be done with the ePWMSYNCI/O.
One other quick question i had is if ePWMSYNC is the same as ePWM4A, or if it's a specifici signal.
Best regards,
Jonathan