Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8305, BOOSTXL-3PHGANINV, INA240, DRV8301
Hi team,
The customer has found some errors in our documents:

As shown above, the LEM overcurrent protection threshold is 11A.

This section of the circuit is shown in the figure, and the sensor output at 11 A of the original side current is calculated as:
LTS 6-NP:( 11 / 3 ) * 0.625 + 2.5 = 4.792V
CAS 6-NP:11 * 2 * 0.1042 + 2.5 = 4.792V
4.792V post-stage operation requires a multiplier of 0.66, i.e. 4.792 * 0.66 = 3.16272V. This voltage value is essentially the same as the 3.1565-V threshold set by the subsequent comparison circuit:

However, for the current sensor, 4.792V is out of the linear range of the sensor output:


Issue: is there anything wrong with the LEM sensor overcurrent protection threshold of 11A described in the document?
Could you help check this case? Thanks.
Best Regards,
Cherry