Part Number: TMS320F280049C
Hi
I‘m using an external CANFD controller for F280049C, I want to use a 20MHz crystal to clock the CAN controller, the CAN controller can output a clock of 20MHz to the MCU X1 pin as an external clock source.
But first I have to use the internal 10MHz of MCU to generate the SPI's clock, and than set the CAN controller's output clock.
Is it Ok that I change the clock's source from internal to external source when MCU normal working?
During the changing time ,will the clock lost effect the CAN FD controller?
Regards
A.W