Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi there,
I'm working on a project for the F28388D CM core. I used one of the driverlib_cm examples as a starting point, so the project includes a reference (linked resource) to driverlib_cm.lib.
In the project there's also a \device folder containing driverlib_cm.h, together with another subfolder \driverlib_cm (excluded from build) containing driverlib_cm source and header files.

Question 1:
Why is this last folder (driverlib_cm *.c and *.h files) included in the project? Wouldn't the project only need the driverlib_cm.lib file and a path to the associated *.h files?
Then in driverlib_cm's sysctl.h there is a definition for the CM clock frequency CM_CLK_FREQ. This definition is used elsewhere in the library for I2C, SSI, and UART calculations. So if the actual CM clock frequency (as set by CPU1) is different, then I need to rebuild the driverlib_cm.lib library.
Question 2:
How do I rebuild driverlib_cm.lib for my project? Please note I don't want to rebuild the lib in the C2000WARE installation folder because another CM project may use a different clock frequency.
Should I use the driverlib_cm source files in the project's \device\driverlib_cm\ folder, and build a project-specific driverlib_cm.lib? Then I would use the local project's driverlib_cm.lib instead of the linked resource in C2000WARE. My only concern then would be to handle updates manually when a new C2000WARE version is released.
I would like to know the recommended working method for such a situation. I can imagine there are more cases where a project-customized driverlib would be needed.
Thanks and kind regards,
Arjan