Hi there,
I'm looking for an explanation of all the predefines that exist in the universal motor control lab code.
The lab's user guide Figure 2-14 Select the Right Pre-define symbols in Project Properties provides a list of the ones that should be active for this lab, and Table 2-4. The Supporting Algorithms, Functions and Motors Matrix in Example Lab gives some of the definitions. But there are more than just these in the code, for example MOTOR1_DECOUP.
I'm looking for an exhaustive list of what these symbols mean and do.
Regards,