Part Number: TMDSDOCK28379D
Hi Team,
We received this inquiry from our customer.
So my problem is that we recently bought the kit TMDSDOCK28379D
We are testing it and we're getting a SINAD lower than indicated in the Microcontroller data sheet when using one of the ADC of the microcontroller.
We would like to know if we're doing something wrong in our test. We would like to know if it is possible to discuss our test setting with someone who can confirm if under this setting we should get the SINAD indicated in the data sheet.
We're getting 60 dB. I wanted to mention the following:
- The signal generator is a NI DAQ USB-6363. We measured its SINAD and we're getting approx. 80 dB.
- Signal Frequency: 1 kHz
- Signal Amplitude 1.6 V.
- Sampling rate of the ADC = 20 K.
Also, In the User Guide of the control card, they recommend for this test to "place additional female SMA connectors on the control card docking station", however, we don't see the appropriate holes to place such SMA connectors in the docking station. We wonder if there is another docking station that we are not aware of.
Regards,
Danilo