This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT: HVPM_Sensorless_2833x.out: a data verification error occurred, file load failed.

Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: TMS320F28335, TMS320F28035, CONTROLSUITE

 Dear Sir, 
I am using  TMDSHVMTRPFCKIT, High Voltage Motor Control and PFC Developer's Kit for my experimental work. I can able to load all the programmers using Piccolo (TMS320F28035) card which is delivered with this board. I am also trying to uses another controller board, delivered with this kit i.e., Delfino (TMS320F28335). When I am debugging the program to this board the following error is coming. 
C28xx: GEL Output: 
Device Calibration not complete, check if device is unlocked and recalibrate.C28xx: Flash Programmer: Warning: The configured device (TMS320F28035), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: GEL Output: 
Device Calibration not complete, check if device is unlocked and recalibrate.C28xx: File Loader: Verification failed: Values at address 0x0825B@Program do not match Please verify target memory and memory map.
C28xx: GEL: File: C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVPM_Sensorless_2833x\F2833x_RAM\HVPM_Sensorless_2833x.out: a data verification error occurred, file load failed.

 Please do the needful. Thanks in advance for your quick support. 

Thanks and Regards

Vineeth