Part Number: TMS320F280039C
Hi Team,
I am trying to see if there is any direct formulae to calculate phase delay between two ePWM modules. When I configure ePWM in both UP mode or both in down mode, I see that phase delay is same as the calculation given in TRM i.e. phase Delay = TBPHS/TBPRD * 360

However, when I want the slave ePWM to be in up - down counter mode, I see that phase delay depends on the counter direction after sync, also the counting mode of the master ePWM.
My question here is, is there a direct formula for phase delay in case of up-down counting in slave?