This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: Consult with the PinMux Example

Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG

Hi Experts,

My customer is using the PinMux to develop the code and found the error as below:

and the C2000 version is the C2000Ware_4_00_00_00.

Step1: when I load the PinMux example as below, and I select the "empty_sysconfig_64qfpq"

Step2: I found the error as below:

Step3: when I click the "Go Back" and Select the below, and it work fine.

So, here are question:

Q1: empty_sysconfig_64qfpq and empty_sysconfig_64qfp, are the two different example?

I have compared the two project file as below, only the difference QFP and QFPQ

Q2: empty_sysconfig_64qfpq If there is a difference, what functions can it be used to specifically implement? Thanks!