Part Number: TMS320F280045
I am very new to software for this TMS320F280045PM part. Our Hardware team just gave me an internally developed board which I need to get software to run on. I can run & debug code from the JTAG emulator but I don't think it is running from a fresh boot without starting from the emulator. The hardware does not have GPIO24 and GPIO32 pulled up with a resistor. The Hardware guys have assigned these to outputs - might be grief if they are pulled high at startup. So I'm pretty sure that without the resistors it is trying to boot from something other than Flash. Is there anything I can do?
Curt