This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Usage of the CLA and DMA

Part Number: TMS320F28379D

Hello,
I have a question regarding the usage of the CLA and DMA. With the bit CPUn.SECMSEL you can choose the connection of the CLA and DMA to the internal bus.



Does that mean it's not possible to use the CLA and DMA at the same time?




Thank you very much

Ralf

  • Hi Ralf,

    Yes, that is correct. . If a peripheral belongs to a CPU subsystem, it can be accessed by the CPU and one of the secondary masters (either DMA or CLA1). The secondary master is statically selected using the SECMSEL register mapped to the respective CPU. 

    Thanks & Regards,

    Santosh