Other Parts Discussed in Thread: CONTROLSUITE
Hi All,
Can F2802X Load code while another application are running or we need customize Boot loader. ?
Thanks
NT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
Hi All,
Can F2802X Load code while another application are running or we need customize Boot loader. ?
Thanks
NT
Knighty Nimp said:Hi All,
Can F2802X Load code while another application are running or we need customize Boot loader. ?
Thanks
NT
NT,
If the question is if the boot ROM loaders (sci, spi, etc) can be interrupted by an application? If so, then yes - the application could call the ROM code and before doing so have interrupts enabled. These are very simple loaders - it just loads a data stream into ROM. The code is available in controlSUITE if you wanted to modify it for your own use.
If instead the question is whether the flash API can be called while an application is running, then the answer is yes as long as the application is completely in RAM. Flash is not available when the API is called, even within an interrupt. This is described in the API documentation (also in controlSUITE www.ti.com/controlsuite).
Regards,
Lori