This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335 I2C FIFO MODE.

Hello All..

I need to create a program that write in I2C more than 16 Bytes....

But I have seen the example that write in a EPROM by I2C but it don't work for mor tah 16 BYTES.

Plz Some one can give to me a example how To use de FIFO to transmit more than 16 BYTES?

 

 

Uint16 I2CA_WriteData(struct I2CMSG *msg)
{
   // Wait until the STP bit is cleared from any previous master communication.
   // Clearing of this bit by the module is delayed until after the SCD bit is
   // set. If this bit is not checked prior to initiating a new message, the
   // I2C could get confused.
   if (I2caRegs.I2CMDR.bit.STP == 1)
   {
      return I2C_STP_NOT_READY_ERROR;
   }
   // Setup slave address
//    I2caRegs.I2CSAR = msg->SlaveAddress;
   // Check if bus busy
   if (I2caRegs.I2CSTR.bit.BB == 1)
   {
      return I2C_BUS_BUSY_ERROR;
   }
   // Setup number of bytes to send
   // MsgBuffer + Address
   I2caRegs.I2CCNT = 7;
   // Setup data to send
 //  I2caRegs.I2CDXR = msg->MemoryHighAddr;
//   I2caRegs.I2CDXR = msg->MemoryLowAddr;
// for (i=0; i<msg->NumOfBytes-2; i++)
I2caRegs.I2CDXR = 0x68;
I2caRegs.I2CDXR = 0x00;
I2caRegs.I2CDXR = 0x03;
I2caRegs.I2CDXR = 0x00;
I2caRegs.I2CDXR = 0x00;
I2caRegs.I2CDXR = 0x00;
I2caRegs.I2CDXR = 0xFF;
    // Send start as master transmitter
   I2caRegs.I2CMDR.all = 0x6E28;
   return I2C_SUCCESS;
}