Part Number: TMS320F28377D
Other Parts Discussed in Thread: ADC12DL040
Hello.
I am trying to do an external ADC using ADC12DL040.
The sampling rate is 10MHz (0.1us).
However, the sampling rate is 2MHz (0.4us).
I am attaching the code and the CCS screen.
Thak you.
Question 1)
Is there any way I can optimize my code?
Question 2)
Even without reading the external ADC there is a lot of delay.
Is there any way to optimize this code?
GPIO_WritePin(MCU_TP2, 1);
GPIO_WritePin(MCU_TP2, 0);
Question3)
Does F28377D (200MHz) take 280ns to turn GPIO ON/OFF?