This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: How to view DCAN Message RAM in CCS

Part Number: TMS320F28388D


I am trying to implement a DCAN interface on the CM core of the TMS320F28388D processor.  I have been successful in transmitting messages but cannot receive any.

I wish to view the Tx and Rx Message Objects in the Message RAM in Code Composer Studio.  I read that when using the debugger that this memory is viewable but I am not able to find it.  The TMS320F2838x Real-Time Microcontrollers With Connectivity Manager Technical Reference Manual (spruii0c) states in Section 30.14 Message RAM: "The message RAM base address is 0x1000 above the base address of the CAN peripheral".

I have tried what I assume should be the correct address but CCS cannot display any memory contents at that location.

For the CM: CANA_BASE =0x4007 0000U so 0x1000 above(?) is either 0x40071000 or 0x4006 F000. Neither location works.

Do I have the correct base address? Is the location different for the CM than for C28x core?

Thanks for your help.