Part Number: TMS320F280049C
Hi all,
I followed this thread to always boot from Flash: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/715617/tms320f280049c-writing-in-otp-memory-to-change-boot-mode-settings
I added this to the linker file:
OTP_BMODE : origin = 0x07800C, length = 0x000001 /* Add by me */ OTP_KEY : origin = 0x07800D, length = 0x000001 /* Add by me */ OTP_Boot : origin = 0x07801C, length = 0x000003 /* Add by me */
and added this at the top of the main.c file:
#pragma DATA_SECTION(OTP_BMODE,"OTP_BMODE"); #pragma DATA_SECTION(OTP_KEY,"OTP_KEY"); #pragma DATA_SECTION(OTP_Boot, "OTP_Boot"); const uint16_t OTP_BMODE = 0x5AFF; <- this is wrong const uint16_t OTP_KEY = 0xFFFF; <- this is wrong const uint16_t OTP_Boot = 0xFF03;
After flashing, the OTP has the expected content:

However the Boot Mode can still be changed with the GPIO. If GPIO24 is held down the code won't boot. Did I miss anything?
Thanks