This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: CCS xds110 and C2prog Unable to Init Driver

Part Number: TMS320F28379D

I am working with CCS v8.3.1, C2Prog  v1.9, XDS110, JTAG, TMS320F28379D, for now just trying to program CPU01. Eventually, I will need to program CPU01, CPU02 and allow OTP programming, but I want to just get this first step of CPU01 programmed done first. 

When I installed C2Prog, I definitely had the TI Emupack checked to install.

I have generated my .hex file. I am not 100% confident I did this correctly, but I did set the flags "--memwidth=16 --romwidth=16 --intel" and it gave me a file.

From there, I've opened up C2prog and have it set up. Firmware image is pointing to my hex file. 

I hit program but I keep getting the error:

I haven't touched the Configure.. Save as ..ehx or Tools.. options, as the C2Prog manual does not mention them in its JTAG programming portion. 

I just can't figure this init driver issue. I've been using the XDS110 within CCS as my debugger with no problem. I followed along the C2Prog manual and completed section 3.3.1 just in case that was the issue. That completed successfully (though note the file in the folder was firmware_3.0.0.13.bin and not just firmware.bin)

I have attempted to follow along with the next section 3.3.2, but the folder c2pemuconf does not exist on my computer. I'm not sure if that is a mistake or points towards I did not install C2Prog correctly, or if there is just somewhere else I should be looking for the config file.  Any ideas?

Along with that, does the issue init driver issue point to an error within C2Prog, or is it possible I still haven't properly created my hex file? 

Any help is appreciated, thank you!