This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Could we create the C28346 chip, in Matlab Simulink??

Other Parts Discussed in Thread: CCSTUDIO

Hi everyone,

I'm currently working on a project using a ti development tool kit. (TMDXDOCK28346-168) I want to use Matlab Simulink to do this project. I want to load the project in the DSP directly from Simulink wich would create the appropriate CCStudio code alone.  But in Matlab Simulink there isn't chip especially for the Delfino C28346, then I have to create them. Could we describe this chip in Matlab Simulink?

I begun to describe the memory pane but I can't understand why there are special bit defined which are not in the data sheet of the component. Secondary for the section configuration I don't know if it's necessary to do any modification or if the chip F28335 has the same section as the C28346? If it's anything to change, I don't know where I've to go to find the different files.

And finally, one more question, in the first part of the configuration, board support, is it necessary to change some path file or them from the F28335 are the same as for the C28346?

 

I'm a beginner in DSP program, thus I don't know all the different trick of the programmer...

Thank you all!!!