Dear Ashwini,
I am trying to implement the following strategy:
- Enable CLA INT X.
- Set for each of the used CLa tasks SOFTINTEN.bit.TaskX to 1 (to avoid end-of-task interrtupt being triggered).
- Monitor each CLA INT X. If it is executed, CLA illegal operation has occured.
I got to know that SOFTINTEN writes should be done in CLA, but I am facing some issues.
is SOFTINTEN keeping its value, or will reset after CLA task execution?
though I am setting SOFTINTEN to 1, End-of-Task is executed, do i need to take into account any other config?
Regarsds,
Marc F