Part Number: TMS320F28374S
Other Parts Discussed in Thread: C2000WARE
Hi.
TMS320F28374S
CCS 11.0.0
C2000Ware 4.0.0.0
1.
I have a board where the pins are hardware pulled up and down: GPIO84 - 1, GPIO72 - 0 (SCI boot mode). R23 missing.
SCI-A: GPIO42 - TX, GPIO43 - RX.
I use the USB-UART converter (FTDI).
I need to program the controller via SCI-A (GPIO42, GPIO43). Is this possible without changing the board layout?
If not, how should the UART-USB converter be connected to a board?
2.
A similar issue with the CAN interface.
CAN-A: GPIO18 - RX, GPIO19 - TX.
Is it possible to program the controller without changing the pins?
Thanks.