Part Number: C2000-GANG
Hi,
I have a question.
My customer has problem with the C2000 GANG as below link.
This thread is closed, so I create a new post.
He has three C2000-GANGs with the same HW version.
One works normally, and the other gangs don't work normally.
When I ran the self-test, one passed and two gangs failed.


Also, one wrote to the target board normally, and the other two had an error.
I think the target board has no problem. Because on the same board one works and the other two don't.
I captured screen when error is occurred.

The gang programmer version in use is as follows.