Part Number: TMS320F280041
Hello,
I'm using the F280041 in a motor control application where sine, cosine, and arctan functions are being used. Because the F280041 has a floating point unit and TMU I'm wondering what the best implementation of these trigonometric functions in regards to accuracy and speed. And, how do I confirm my C code is configured to use that 'best implementation'. Because of the presence of the FPU most of the working variables are of type float32_t.
Is there a guidance document that can help me understand this?
Thanks - Bruce