Other Parts Discussed in Thread: C2000WARE
I tried SCI Boot loading in TMS320F28377D microcontroller development board.
Initially I changed the SW1 switch positions for SCI Boot mode in development board.
I created the .txt files which are required for bootloading through serial flash programmer using hex2000 utility
In serial flash programmer I gave the command for bootloading.
serial_flash_programmer.exe -d f2837xD -k F2837xD_sci_flash_kernels_cpu01.txt -a blinky_cpu01.txt -p COM7 -b 9600.
after this command it has to show the options for FLASH erasing and loading ,but it is showing that flash kernel is downloading and it is stucking there only.
The image about the issue is attatched below.
Please help me with this issue.