Part Number: 2MTR-DYNO
www.ti.com/.../2MTR-DYNO This motors.
I wanted to control the speed of the Teknic motor M-2310P-LN-04K.
Before I started with the closed loop I used the open loop to check the hall and encoder signals.
Unfortunately the Encoder signals are always at almost 5 V and they don't change when the motor rotates. On the contrary to hall signals which are changing when the motor rotates. For Hall and Encoder interface I used the configuration de.mathworks.com/.../hardware-connections.html
Both motors with SN:520671C and SN:519440C have the same problem. I have a third motor with SN: 465119C, whose encoder interface works with the same setting.
The motor is not working. We are supplying 5V for the encoder. But no signal arrives on the terminal of the encoder.
I think the encoder is damaged. We did a simple test only supplying 5 V and rotating the motor by hand.
The old motor we had was working by hand as well as with the inverter used. I do have the old one and it works properly. With the same setup both new motors are not working.
Anything I’m missing?