Other Parts Discussed in Thread: C2000WARE
I have tried using the USB serial port to load a hex file on to the Launchpad kit with F280049C processor, but with no success. This is all the print out I get:
C2000 Serial Firmware Upgrader
Copyright (c) 2021 Texas Instruments Incorporated. All rights reserved.
getting comm state
building comm DCB
adjusting port settings
calling f021_DownloadKernel CPU1 Kernel
Downloading flashapi_sci_kernel.txt to device...
The serial programmer sits there forever (at least 5 minutes or more). There are no flashing leds to indicate download is proceeding.
Here is the command line i am using:
.\sfp.exe -d f28004x -k flashapi_sci_kernel.txt -a MCE.hex -p COM10 -b 115200
where i renamed seriail programmer as sfp.exe.
I found the serial programmer in the following TI install directory:
c:\ti\c2000\C2000Ware_4_00_00\utilities\flash_programmers\serial_flash_programmer
Of course, the boot dip switch is set for SCI (actually I have tried every possible combo with same result).
Okay, got any help to give me?!!! Why does it just sit there.