Part Number: TMS320F28379D
In the F2837xD_usb_flash_kernels_cpu01 example, There is USB_Boot.c
Here is the code for Peripheral Software Reset as shown in the picture below.

I don't understand what USB_A represents in this code.
I wonder if this code works when the USB connect to J8 is connected to the PC. If I don't connect J8 USB Connector, Can't I use the example above?