This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Can microcontroller boot up faster than 250 ms from internal flash?

Part Number: TMS320F28377S

Hi,

It seems TI Boot ROM execution takes 250 ms during power up. Time was measured from external 3.3V signal to first possible I/O control with oscilloscope.

Questions:

1) Can device boot up faster than 250 ms from internal flash?

2) How long should it take to boot up microcontroller, worst-case / typical TI Boot ROM execution?

Best regards,

Juhamatti Nikander