Part Number: DRV8301-HC-C2-KIT
Hello,
We've been trying to implement the Lab 2a with the "TI DRV8301-HC-C2-KIT" board. The connections are correct, but the motor doesn't move during the identification. Besides, the process fails during EST_State_Ls and the control and estimator enter in error (CTRL_State_Error and EST_State_Error), and the Rs and flux values are too high.
These are the overall values:

We don't know if the problem is caused due to software (the code is Lab 2a as it is) or may be a hardware problem.
Thanks for the attention.