Part Number: TMS320F28335
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ao,
This query has been assigned to the expert. Please expect delay in response due to the US holiday on Monday.
Thanks
Vasudha
Ao,
The features listed are capabilities of the CPU core. This does not mean all these capabilities are implemented as features in the device. Many C2000 devices don’t even have the EMU0/EMU1 pins. Note the line above the table "A target system is not required to support any mode other than normal mode." Only Normal mode is implemented in this device.
Do you mean that the TMS320F28335 chip does not have a slave mode of Device Operating Modes? which chip it can be work on?
"A target system is not required to support any mode other than normal mode." Only Normal mode is implemented in this device.------yes! But the "Wait-in-reset" mode and the " Reserved for testing" mode are implemented in the 28335 device,why the slave mode is special?
Do you mean that the TMS320F28335 chip does not have a slave mode of Device Operating Modes?
Correct.
which chip it can be work on?
No C2000 device supports this mode.
You can refer to SPRU430 for learning more about the instruction set, pipeline etc. For device-specific capabilities, please refer only to the datasheet www.ti.com/lit/SPRS439.