Part Number: TMS320F280039C
Dear Champs,
I am asking this for our customer.
Is it possible to use communication peripheral to trigger CLB?
For example, I2C stop bit to trigger CLB and then use CLB to check I2C RX buffer with some logic combination?
For example, SCI stop bit to trigger CLB and then use CLB to check SCI RX buffer with some logic combination?
DMA may be used as well.
The goal is to reduce CPU loading and use peripheral/CLB/DMA a routine check on its data.
Do you have any idea or suggestion?
Wayne Huang