This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Hardware Dependent Files - Going from Dev Board with 100 Pin to 56 Pin Package

Part Number: TMS320F280049C
Other Parts Discussed in Thread: MOTORWARE

Hello,

From my understanding motorware is laid out in such a way where all hardware specific definitions are within hal.h, hal.c, user.h, and user.c.  As we are transition from firmware written for the f28004 dev board which uses the 100 pin to now the 56 pin configuration we are forced to use different ADCs/GPIOS as some do not exist.  Are there any other files we should look into when making this hardware change?

It is worth noting that we are using the same DRV as used with the Dev Board.

Thanks,
Jonathan