This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the program could not run to _c_int00

my project is rtsc Flashbios based under ccsv4.1.2,my platfrom is ezdsp28335,i compiled ok,but when i download the .out program.it could not run to main.i debug find that it run to   

 .sect "codestart"
code_start:
    .if WD_DISABLE == 1
        LB wd_disable       ;Branch to watchdog disable code
    .else
        LB _c_int00         ;Branch to start of boot.asm in RTS library
    .endif

but it could not run to _c_int00         .i could see _c_int00    asm : all is ffff code.

          _c_int00:
0x304ADA:   FFFF        ITRAP1
0x304ADB:   FFFF        ITRAP1
0x304ADC:   FFFF        ITRAP1
0x304ADD:   FFFF        ITRAP1
0x304ADE:   FFFF        ITRAP1
what reasons do   result the  problem.