Hi champs,
I am asking for our customer. And the customer needs extra pin for GPIO(64-pin PM version ), is it a way to use the TDO as I2CA_SCL ?

First, when load the code to flash by the JTAG emulator(TDO, TDI, TMS, and TCK), and then when in the standalone mode (without JTAG emulator), the TDO used as the I2CA_SCL, am I correct?
Only need to be re-configured in SW as below, and design for multiplexing on hardware:

Are there other considerations/Concern? BTW, customer need JTAG, Nor consider cJTAG. Thanks~