Part Number: TMS320F280041
HI,
I am having an issue with the XDS110 Debug probe wherein the debugger randomly disconnects while the board is in operation. I am using a 4-wrie JTAG protocol with a 14-pin connector
A few observations about the problem.
- The problem occurs usually while the debugging session is in progress and not during code upoad.
- The time duration after which the disconnection happens is entirely random. Sometimes the connection will for fine for 5 minutes and on other occasions it fails within a few seconds.
- Swapping the cable from the debugger to the laptop or the cable from the debugger to the micro-controller does not solve the issue.
- After the debugger disconnects once it's not possible to enter a debugging session again unless I power cycle the micro-controller.
Console Log of the error.
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129)
C28xx_CPU1: Trouble Halting TargetCPU: (Error -1135 @ 0x82469) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129)
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debuggingng
Solutions to the issue and suggestions on how to make the connection more reliable will be appreciated
Regards,
Parth
WCB Robotics.