This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: How to debug user application with XDS 110

Part Number: TMS320F280039C

Hello, 

I have the current setup - I have the TMS320F280039C and docking station with an external XDS110 plugged into the docking station. This setup works to load the led_ex1_blinky project. 

In the led_ex1_blinky project the correct probe is selected

But in my user project the XDS100v1 is selected instead of the XDS110. How do I select the XDS110? I want to load my user application to the development board to make sure I can step through the code while I'm waiting on my actual hardware

Thanks for the help!