Part Number: TMS320F280023
Hi there,
I would like to use MAX3098E IC with TMS320F280023 MCU. We're using OUTZ pin as a index pin. Should I connect the OUTZ pin to the MCU timer or should I connect it as a normal I/O pin ?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280023
Hi there,
I would like to use MAX3098E IC with TMS320F280023 MCU. We're using OUTZ pin as a index pin. Should I connect the OUTZ pin to the MCU timer or should I connect it as a normal I/O pin ?

Hello,
We're using OUTZ pin as a index pin. Should I connect the OUTZ pin to the MCU timer or should I connect it as a normal I/O pin ?
I'm assuming you will be using the eQEP module on the MCU. The Index pin should be connected to eQEP-I pin on the MCU.
Regards
Lori