Other Parts Discussed in Thread: TMS320F2812
Hi All,
Can anyone help?
I have a number of boards based on the TMS320F2812 which I need to program via SDflash.
The boards are clocked from 30Mhz and the CPU_rate is set to 6.67 however, when I run the SDFlash toggle test with the frequency on mdxa pin is approx 3Mhz not the 10Khz as specified in the SD flash ref guide.
The SDflash algorithm files are set up correctly with the correct rates eg 30Mhz, PLLCR = 10 , I just dont understand why Iam getting 3Mhz and not 10Khz
Consequently the devices fail to program.
If try the same experiment on my ezdsp dev board the toggle test works at 10Khz and I can program the flash
Anybody go any ideas I would greatly appreciate it?