Part Number: TMDSCNCD280049C
Other Parts Discussed in Thread: C2000WARE,
Hi Team,
When I use C2000Ware_3_04_00_00\driverlib\f28004x\examples\adcadc_ex11_multiple_soc_epwm , I can read ADC_result of ADC module A , but the ADC_result of ADC module C has no changed value in Debug Mode of CCS. The ADC_result of ADC module C is always zero.
I want to feedback the ADC result of module A and C (or B) synchronously.
My Progress is using TMDSCNCD280049C to feedback differential AD value.
Because 280049C has synchronous singal end ADC converters, I want to use two ADC converter( like module A and B )
to feedback differential signal synchronously.
And then subtracting the other to get differential ADC value.
This direction is right ?

Pls check it.
Thanks Regards.
James