Part Number: TMS320F280025C
Other Parts Discussed in Thread: TIDM-02000
I am trying to PCMC_PSFB used F280025 with reference to TIDM-02000.(Example Projects:TIDM-02000-Peak Current Controlled Mode PSFB DC-DC Power Converter)
It works fine normally, but I have a problem and I want to solve.
The waveform immediately after enabling PWM is not ideal.
As shown in the figure below, [Q1 and Q3] or [Q2 and Q4] are turned on at the same time.
At this time, current will flow to the primary side.
The waveform from the second cycle is ideal for me.
How can I output a waveform like the second cycle from the beginning?


I haven't changed much from the Example Project.
The settings are as follows.
PSFB_INCR_BUILD = 2 (Closed Voltage Loop Check)
PSFB_SR_mode = 1
Dead-Band = 1us(Temporary setting)
PWM frequency = 100kHz
The PWM enable method is as follows.
(Same as Example Project)

Is it possible that one of the causes of this problem is that PWM2 is always output?
If so, do you know a good way to stop the PWM2 output?
Regards,
Masaru,