Part Number: C2000WARE-DIGITALPOWER-SDK
Other Parts Discussed in Thread: POWERSUITE, TIDM-1000, C2000WARE,
Hello,
I am following the design guide for the TIDM-1000. It says to install the DigitalPower SDK. I did that. It says that on re-launch of CCS, "CCS will automatically detect powerSUITE".
(1) How do I know if CCS actually detected powerSUITE? I can't find anything that explains how I know if CCS actually detected it.
It then says to open the Resource Explorer and navigate to the relevant project for the TIDM-1000. So in this case it is under Software->C2000Ware_DigitalPower_SDK->Example Project->F2837x. Great found it. But the design guide says to click "Run <device> Project".
(2) I don't see that anywhere. Where do I find "Run <device> Project"?
Then I tried to click "Import F28379D Project". I get a message saying Cannot Import Project because the package needs to be install locally. I assume that the "package" is the DigitalPower SDK. But I already did that! So I assume that I installed the SDK to the wrong location and CCS can't find it.
(3) What folder path should the DigitalPower SDK be installed so that CCS can see it?
Good news! It asks "Would you like to install it now"? I click Install. It says that it will be installed in the background. And that progress can be viewed using the "task view, accessible from the toolbar".
(4) What is the task view? What toolbar?
I suspect that it is not actually installing the background but I can't be sure because I can't find this task view.
Please help!
Kevin
Kevin