Part Number: TMS320F2812
Hello,
My question is related to the "ways of working" with the eCAN interface.
TMS320F2812 has a single eCAN with 32 mailbox. It need to communicate with 30 nodes in a master-slave scheme.
The interrogation time is not the same for all nodes. It depends on the type of the node.
As there are more nodes than mailboxes I will have to change the configurations of the mailboxes dynamically.
Is it a problem?
Thanks in advance for the response.
Marcio Borges