Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
Dear All,
I am trying to generate complementary PMW using digital power template /library. However, the EPWMB always shows high.
I am attaching the template file, asm.and related c code.
The main code is
//----------------------------------------------------------------------------------
// FILE: ProjectName-Main.C
//
// Description: Sample Template file to edit
// The file drives duty on PWM1A using C28x
// These can be deleted and modifed by the user
// C28x ISR is triggered by the PWM 1 interrupt
//
// Version: 2.0
//
// Target: TMS320F2802x(PiccoloA),
//
//----------------------------------------------------------------------------------
// Copyright Texas Instruments © 2004-2010
//----------------------------------------------------------------------------------
// Revision History:
//----------------------------------------------------------------------------------
// Date | Description / Status
//----------------------------------------------------------------------------------
// October 2010 - Sample template project with DPLib v3 (MB)
//----------------------------------------------------------------------------------
//
// PLEASE READ - Useful notes about this Project
// Although this project is made up of several files, the most important ones are:
// "{ProjectName}-Main.C" - this file
// - Application Initialization, Peripheral config,
// - Application management
// - Slower background code loops and Task scheduling
// "{ProjectName}-DevInit_F28xxx.C
// - Device Initialization, e.g. Clock, PLL, WD, GPIO mapping
// - Peripheral clock enables
// - DevInit file will differ per each F28xxx device series, e.g. F280x, F2833x,
// "{ProjectName}-DPL-ISR.asm
// - Assembly level library Macros and any cycle critical functions are found here
// "{ProjectName}-DPL-CLA.asm"
// - Init code for DPlib CLA Macros run by C28x
// - CLA Task code
// "{ProjectName}-Settings.h"
// - Global defines (settings) project selections are found here
// - This file is referenced by both C and ASM files.
// "{ProjectName}-CLAShared.h.h"
// - Variable defines and header includes that are shared b/w CLA and C28x
//
// Code is made up of sections, e.g. "FUNCTION PROTOTYPES", "VARIABLE DECLARATIONS" ,..etc
// each section has FRAMEWORK and USER areas.
// FRAMEWORK areas provide useful ready made "infrastructure" code which for the most part
// does not need modification, e.g. Task scheduling, ISR call, GUI interface support,...etc
// USER areas have functional example code which can be modified by USER to fit their appl.
//
// Code can be compiled with various build options (Incremental Builds IBx), these
// options are selected in file "{ProjectName}-Settings.h". Note: "Rebuild All" compile
// tool bar button must be used if this file is modified.
//----------------------------------------------------------------------------------
#include "ProjectName-Settings.h"
#include "PeripheralHeaderIncludes.h"
#include "DSP2802x_EPWM_defines.h"
#include "DPlib.h"
#include "IQmathLib.h"
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// FUNCTION PROTOTYPES
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// Add protoypes of functions being used in the project here
void DeviceInit(void);
#ifdef FLASH
void InitFlash();
#endif
void MemCopy();
//-------------------------------- DPLIB --------------------------------------------
//void PWM_1ch_CNF(int16 n, int16 period, int16 mode, int16 phase); For one channel only (A)
void PWM_ComplPairDB_CNF(int16 n, int16 period, int16 mode, int16 phase);// for one channel A,B (Complementary)
void PWM_ComplPairDB_UpdateDB(int16 n,int16 dbRed, int16 dbFed);
void ADC_SOC_CNF(int ChSel[], int Trigsel[], int ACQPS[], int IntChSel, int mode);
// -------------------------------- FRAMEWORK --------------------------------------
// State Machine function prototypes
//----------------------------------------------------------------------------------
// Alpha states
void A0(void); //state A0
void B0(void); //state B0
void C0(void); //state C0
// A branch states
void A1(void); //state A1
void A2(void); //state A2
void A3(void); //state A3
void A4(void); //state A4
// B branch states
void B1(void); //state B1
void B2(void); //state B2
void B3(void); //state B3
void B4(void); //state B4
// C branch states
void C1(void); //state C1
void C2(void); //state C2
void C3(void); //state C3
void C4(void); //state C4
// Variable declarations
void (*Alpha_State_Ptr)(void); // Base States pointer
void (*A_Task_Ptr)(void); // State pointer A branch
void (*B_Task_Ptr)(void); // State pointer B branch
void (*C_Task_Ptr)(void); // State pointer C branch
//----------------------------------------------------------------------------------
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// VARIABLE DECLARATIONS - GENERAL
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// -------------------------------- FRAMEWORK --------------------------------------
int16 VTimer0[4]; // Virtual Timers slaved off CPU Timer 0
int16 VTimer1[4]; // Virtual Timers slaved off CPU Timer 1
int16 VTimer2[4]; // Virtual Timers slaved off CPU Timer 2
// Used for running BackGround in flash, and ISR in RAM
extern Uint16 *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart;
// Used for copying CLA code from load location to RUN location
extern Uint16 Cla1funcsLoadStart, Cla1funcsLoadEnd, Cla1funcsRunStart;
// Used for ADC Configuration
int ChSel[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
int TrigSel[16] = {0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
int ACQPS[16] = {7,7,7,7,7,7,7,7,7,7,7,7,7,7,7,7};
// Used to indirectly access all EPWM modules
volatile struct EPWM_REGS *ePWM[] =
{ &EPwm1Regs, //intentional: (ePWM[0] not used)
&EPwm1Regs,
&EPwm2Regs,
&EPwm3Regs,
&EPwm4Regs,
};
// Used to indirectly access all Comparator modules
volatile struct COMP_REGS *Comp[] =
{ &Comp1Regs, //intentional: (Comp[0] not used)
&Comp1Regs,
&Comp2Regs,
};
// ---------------------------------- USER -----------------------------------------
// ---------------------------- DPLIB Net Pointers ---------------------------------
// Declare net pointers that are used to connect the DP Lib Macros here
// PWMDRV_1ch
//extern volatile long *PWMDRV_1ch_Duty1; // instance #1, EPWM1
extern volatile long *PWMDRV_ComplPairDB_Duty1;
extern volatile long *CNTL_2P2Z_Ref1;
extern volatile long *CNTL_2P2Z_Fdbk1;
extern volatile long *CNTL_2P2Z_Out1;
extern volatile long *CNTL_2P2Z_Coef1;
// ---------------------------- DPLIB Variables ---------------------------------
// Declare the net variables being used by the DP Lib Macro here
volatile long Duty1;
volatile long Net2;
/* Digital Power (DP) Library Initialization */
//DPL_Init(); // Initialize DP Library
//Feedback node connections
//ADCDRV_1ch_R1t0= &Net2;
//CNTL_2P2Z_Fdbk1= &Net2;
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// VARIABLE DECLARATIONS - CCS WatchWindow / GUI support
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// -------------------------------- FRAMEWORK --------------------------------------
//GUI support variables
// sets a limit on the amount of external GUI controls - increase as necessary
int16 *varSetTxtList[16]; //16 textbox controlled variables
int16 *varSetBtnList[16]; //16 button controlled variables
int16 *varSetSldrList[16]; //16 slider controlled variables
int16 *varGetList[16]; //16 variables sendable to GUI
int16 *arrayGetList[16]; //16 arrays sendable to GUI
int16 LedBlinkCnt;
// ---------------------------------- USER -----------------------------------------
// Monitor ("Get") // Display as:
// Configure ("Set")
// History arrays are used for Running Average calculation (boxcar filter)
// Used for CCS display and GUI only, not part of control loop processing
//Scaling Constants (values found via spreadsheet; exact value calibrated per board)
// Variables for background support only (no need to access)
int16 i; // common use incrementer
Uint32 HistPtr, temp_Scratch; // Temp here means Temporary
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// MAIN CODE - starts here
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
void main(void)
{
//=================================================================================
// INITIALISATION - General
//=================================================================================
// The DeviceInit() configures the clocks and pin mux registers
// The function is declared in {ProjectName}-DevInit_F2803/2x.c,
// Please ensure/edit that all the desired components pin muxes
// are configured properly that clocks for the peripherals used
// are enabled, for example the individual PWM clock must be enabled
// along with the Time Base Clock
DeviceInit(); // Device Life support & GPIO
//-------------------------------- FRAMEWORK --------------------------------------
// Only used if running from FLASH
// Note that the variable FLASH is defined by the compiler with -d FLASH
#ifdef FLASH
// Copy time critical code and Flash setup code to RAM
// The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
// symbols are created by the linker. Refer to the linker files.
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
InitFlash(); // Call the flash wrapper init function
#endif //(FLASH)
// Timing sync for background loops
// Timer period definitions found in PeripheralHeaderIncludes.h
CpuTimer0Regs.PRD.all = mSec1; // A tasks
CpuTimer1Regs.PRD.all = mSec10; // B tasks
CpuTimer2Regs.PRD.all = mSec100; // C tasks
// Tasks State-machine init
Alpha_State_Ptr = &A0;
A_Task_Ptr = &A1;
B_Task_Ptr = &B1;
C_Task_Ptr = &C1;
VTimer0[0] = 0;
VTimer1[0] = 0;
VTimer2[0] = 0;
LedBlinkCnt = 5;
// ---------------------------------- USER -----------------------------------------
// put common initialization/variable definitions here
//===============================================================================
// INITIALISATION - GUI connections
//=================================================================================
// Use this section only if you plan to "Instrument" your application using the
// Microsoft C# freeware GUI Template provided by TI
/*
//"Set" variables
//---------------------------------------
// assign GUI variable Textboxes to desired "setable" parameter addresses
varSetTxtList[0] = &Gui_TxtListVar;
varSetTxtList[1] = &Gui_TxtListVar;
varSetTxtList[2] = &Gui_TxtListVar;
varSetTxtList[3] = &Gui_TxtListVar;
varSetTxtList[4] = &Gui_TxtListVar;
varSetTxtList[5] = &Gui_TxtListVar;
varSetTxtList[6] = &Gui_TxtListVar;
varSetTxtList[7] = &Gui_TxtListVar;
varSetTxtList[8] = &Gui_TxtListVar;
varSetTxtList[9] = &Gui_TxtListVar;
varSetTxtList[10] = &Gui_TxtListVar;
varSetTxtList[11] = &Gui_TxtListVar;
// assign GUI Buttons to desired flag addresses
varSetBtnList[0] = &Gui_BtnListVar;
varSetBtnList[1] = &Gui_BtnListVar;
varSetBtnList[2] = &Gui_BtnListVar;
varSetBtnList[3] = &Gui_BtnListVar;
varSetBtnList[4] = &Gui_BtnListVar;
// assign GUI Sliders to desired "setable" parameter addresses
varSetSldrList[0] = &Gui_SldrListVar;
varSetSldrList[1] = &Gui_SldrListVar;
varSetSldrList[2] = &Gui_SldrListVar;
varSetSldrList[3] = &Gui_SldrListVar;
varSetSldrList[4] = &Gui_SldrListVar;
//"Get" variables
//---------------------------------------
// assign a GUI "getable" parameter address
varGetList[0] = &Gui_GetListVar;
varGetList[1] = &Gui_GetListVar;
varGetList[2] = &Gui_GetListVar;
varGetList[3] = &Gui_GetListVar;
varGetList[4] = &Gui_GetListVar;
varGetList[5] = &Gui_GetListVar;
varGetList[6] = &Gui_GetListVar;
varGetList[7] = &Gui_GetListVar;
varGetList[8] = &Gui_GetListVar;
varGetList[9] = &Gui_GetListVar;
varGetList[10] = &Gui_GetListVar;
varGetList[11] = &Gui_GetListVar;
varGetList[12] = &Gui_GetListVar;
varGetList[13] = &Gui_GetListVar;
varGetList[14] = &Gui_GetListVar;
varGetList[15] = &Gui_GetListVar;
// assign a GUI "getable" parameter array address
arrayGetList[0] = &DBUFF1; //only need to set initial position of array,
arrayGetList[1] = &DBUFF2; // program will run through it accordingly
arrayGetList[2] = &DBUFF3;
arrayGetList[3] = &DBUFF4;
*/
//==================================================================================
// INCREMENTAL BUILD OPTIONS - NOTE: selected via {ProjectName-Settings.h
//==================================================================================
// ---------------------------------- USER -----------------------------------------
//----------------------------------------------------------------------
#if (INCR_BUILD == 1) // Open Loop Two Phase Interleaved PFC PWM Driver
//----------------------------------------------------------------------
// Configure ADC to be triggered from EPWM1 Period event
//Map channel to ADC Pin
ChSel[0]=14; //Map channel 0 to pin ADC-B6
// for additional ADC conversions modify below
/*ChSel[1]=n; //An
ChSel[2]=n; //An
ChSel[3]=n; //An
ChSel[4]=n; //An
ChSel[5]=n; //An
ChSel[6]=n; //An
ChSel[7]=n; //An
ChSel[8]=n; //An
ChSel[9]=n; //An
ChSel[10]=n; //An
ChSel[11]=n; //An
ChSel[12]=n; //An
ChSel[13]=n; //An
ChSel[14]=n; //An
ChSel[15]=n; //An
*/
// Select Trigger Event for ADC conversion
TrigSel[0]= ADCTRIG_EPWM1_SOCA;
// associate the appropriate peripheral trigger to the ADC channel
/*TrigSel[1]= ADCTRIG_EPWMn_SOCA;
TrigSel[2]= ADCTRIG_EPWMn_SOCA;
TrigSel[3]= ADCTRIG_EPWMn_SOCA;
TrigSel[4]= ADCTRIG_EPWMn_SOCA;
TrigSel[5]= ADCTRIG_EPWMn_SOCA;
TrigSel[6]= ADCTRIG_EPWMn_SOCA;
TrigSel[7]= ADCTRIG_EPWMn_SOCA;
TrigSel[8]= ADCTRIG_EPWMn_SOCA;
TrigSel[9]= ADCTRIG_EPWMn_SOCA;
TrigSel[10]= ADCTRIG_EPWMn_SOCA;
TrigSel[11]= ADCTRIG_EPWMn_SOCA;
TrigSel[12]= ADCTRIG_EPWMn_SOCA;
TrigSel[13]= ADCTRIG_EPWMn_SOCA;
TrigSel[14]= ADCTRIG_EPWMn_SOCA;
TrigSel[15]= ADCTRIG_EPWMn_SOCA;*/
// Configure PWM1 for 200Khz (Period Count= 60Mhz/200Khz = 300)
PWM_ComplPairDB_CNF(1,600, 1, 0);
PWM_ComplPairDB_UpdateDB(1,10,10);
// Configure the ADC with auto interrupt clear mode
// ADC interrupt after EOC of channel 0
ADC_SOC_CNF(ChSel,TrigSel,ACQPS,0,2);
// Configure the EPWM1 to issue the SOC
EPwm1Regs.ETSEL.bit.SOCAEN = 1;
EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_PRD; // Use PRD event as trigger for ADC SOC
EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; // Generate pulse on every event
// Digital Power CLA(DP) library initialisation
DPL_Init();
// Lib Module connection to "nets"
//----------------------------------------
// Connect the PWM Driver input to an input variable, Open Loop System
PWMDRV_ComplPairDB_Duty1 = &Duty1;
Duty1 =_IQ24(0.5);
PWM_ComplPairDB_UpdateDB(1,10,10);
// Initialize the net variables
#endif // (INCR_BUILD == 1)
//====================================================================================
// INTERRUPTS & ISR INITIALIZATION (best to run this section after other initialization)
//====================================================================================
// Set up C28x Interrupt
//Also Set the appropriate # define's in the {ProjectName}-Settings.h
//to enable interrupt management in the ISR
EALLOW;
PieVectTable.EPWM1_INT = &DPL_ISR; // Map Interrupt
PieCtrlRegs.PIEIER3.bit.INTx1 = 1; // PIE level enable, Grp3 / Int1
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // INT on PRD event
EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on every event
IER |= M_INT3; // Enable CPU INT3 connected to EPWM1-6 INTs:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
EDIS;
//=================================================================================
// BACKGROUND (BG) LOOP
//=================================================================================
//--------------------------------- FRAMEWORK -------------------------------------
for(;;) //infinite loop
{
// State machine entry & exit point
//===========================================================
(*Alpha_State_Ptr)(); // jump to an Alpha state (A0,B0,...)
//===========================================================
}
} //END MAIN CODE
//=================================================================================
// STATE-MACHINE SEQUENCING AND SYNCRONIZATION
//=================================================================================
//--------------------------------- FRAMEWORK -------------------------------------
void A0(void)
{
// loop rate synchronizer for A-tasks
if(CpuTimer0Regs.TCR.bit.TIF == 1)
{
CpuTimer0Regs.TCR.bit.TIF = 1; // clear flag
//-----------------------------------------------------------
(*A_Task_Ptr)(); // jump to an A Task (A1,A2,A3,...)
//-----------------------------------------------------------
VTimer0[0]++; // virtual timer 0, instance 0 (spare)
}
Alpha_State_Ptr = &B0; // Comment out to allow only A tasks
}
void B0(void)
{
// loop rate synchronizer for B-tasks
if(CpuTimer1Regs.TCR.bit.TIF == 1)
{
CpuTimer1Regs.TCR.bit.TIF = 1; // clear flag
//-----------------------------------------------------------
(*B_Task_Ptr)(); // jump to a B Task (B1,B2,B3,...)
//-----------------------------------------------------------
VTimer1[0]++; // virtual timer 1, instance 0 (spare)
}
Alpha_State_Ptr = &C0; // Allow C state tasks
}
void C0(void)
{
// loop rate synchronizer for C-tasks
if(CpuTimer2Regs.TCR.bit.TIF == 1)
{
CpuTimer2Regs.TCR.bit.TIF = 1; // clear flag
//-----------------------------------------------------------
(*C_Task_Ptr)(); // jump to a C Task (C1,C2,C3,...)
//-----------------------------------------------------------
VTimer2[0]++; //virtual timer 2, instance 0 (spare)
}
Alpha_State_Ptr = &A0; // Back to State A0
}
//=================================================================================
// A - TASKS
//=================================================================================
//--------------------------------------------------------
void A1(void)
//--------------------------------------------------------
{
//-------------------
//the next time CpuTimer0 'counter' reaches Period value go to A2
A_Task_Ptr = &A2;
//-------------------
}
//-----------------------------------------------------------------
void A2(void)
//-----------------------------------------------------------------
{
//-------------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A3;
//-------------------
}
//-----------------------------------------
void A3(void)
//-----------------------------------------
{
//-----------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A4;
//-----------------
}
//----------------------------------------------------------
void A4(void)
//---------------------------------------------------------
{
//-----------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A1;
//-----------------
}
//=================================================================================
// B - TASKS
//=================================================================================
//----------------------------------- USER ----------------------------------------
//----------------------------------------
void B1(void)
//----------------------------------------
{
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B2
B_Task_Ptr = &B2;
//-----------------
}
//----------------------------------------
void B2(void) // Blink LED on the control CArd
//----------------------------------------
{
if(LedBlinkCnt==0)
{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; //turn on/off LD3 on the controlCARD
LedBlinkCnt=5;
}
else
LedBlinkCnt--;
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B3
B_Task_Ptr = &B3;
//-----------------
}
//----------------------------------------
void B3(void)
//----------------------------------------
{
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B4
B_Task_Ptr = &B4;
//-----------------
}
//----------------------------------------
void B4(void) // SPARE
//----------------------------------------
{
//-----------------
//the next time CpuTimer1 'counter' reaches Period value go to B1
B_Task_Ptr = &B1;
//-----------------
}
//=================================================================================
// C - TASKS
//=================================================================================
//--------------------------------- USER ------------------------------------------
//------------------------------------------------------
void C1(void)
//------------------------------------------------------
{
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C2
C_Task_Ptr = &C2;
//-----------------
}
//----------------------------------------
void C2(void)
//----------------------------------------
{
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C3
C_Task_Ptr = &C3;
//-----------------
}
//-----------------------------------------
void C3(void)
//-----------------------------------------
{
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C4
C_Task_Ptr = &C4;
//-----------------
}
//-----------------------------------------
void C4(void) // SPARE
//-----------------------------------------
{
//-----------------
//the next time CpuTimer2 'counter' reaches Period value go to C1
C_Task_Ptr = &C1;
//-----------------
}
The c file for PWM is
//----------------------------------------------------------------------------------
// FILE: PWM_ComplPairDB_Cnf.c
//
// Description: PWM configuration function for complimentary waveform on A & B
// with dead band
//
// Version: 2.0
//
// Target: TMS320F2802x,
// TMS320F2803x,
//
// The function call is:
//
// PWM_ComplPairDB_CNF(int16 n, int16 period, int16 mode, int16 phase)
//
// Function arguments defined as:
//-------------------------------
// n = Target ePWM module, 1,2,...16. e.g. if n=2, then target is ePWM2
// period = PWM period in Sysclks
// mode = Master/Slave mode, e.g. mode=1 for master, mode=0 for slave
// phase = phase offset from upstream master in Sysclks,
// applicable only if mode=0, i.e. slave
//--------------------------------------------------------------------------------
#include "PeripheralHeaderIncludes.h"
#include "DSP2802x_EPWM_defines.h"
extern volatile struct EPWM_REGS *ePWM[];
void PWM_ComplPairDB_CNF(int16 n, int16 period, int16 mode, int16 phase)
{
// Time Base SubModule Registers
(*ePWM[n]).TBCTL.bit.PRDLD = TB_SHADOW; // set load on CTR=0
(*ePWM[n]).TBPRD = period-1; // PWM frequency = 1 / period
(*ePWM[n]).TBPHS.half.TBPHS = 0;
(*ePWM[n]).TBCTR = 0;
(*ePWM[n]).TBCTL.bit.CTRMODE = TB_COUNT_UP;
(*ePWM[n]).TBCTL.bit.HSPCLKDIV = TB_DIV1;
(*ePWM[n]).TBCTL.bit.CLKDIV = TB_DIV1;
if (mode == 1) // config as a Master
{
(*ePWM[n]).TBCTL.bit.PHSEN = TB_DISABLE;
(*ePWM[n]).TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // sync "down-stream"
}
if (mode == 0) // config as a Slave (Note: Phase+2 value used to compensate for logic delay)
{
(*ePWM[n]).TBCTL.bit.PHSEN = TB_ENABLE;
(*ePWM[n]).TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
if ((0 <= phase)&&(phase <= 2)) (*ePWM[n]).TBPHS.half.TBPHS = (2-phase);
if (phase > 2) (*ePWM[n]).TBPHS.half.TBPHS = (period-phase+2);
}
// Counter Compare Submodule Registers
(*ePWM[n]).CMPA.half.CMPA = 0; // set duty 0% initially
//(*ePWM[n]).CMPB = 0; // set duty 0% initially
(*ePWM[n]).CMPCTL.bit.SHDWAMODE = CC_SHADOW;
(*ePWM[n]).CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
(*ePWM[n]).CMPCTL.bit.SHDWBMODE = CC_SHADOW;// edited on 13-06-2022 (this line was not present in original)
(*ePWM[n]).CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;// edited on 13-06-2022 (this line was not present in original)
// Action Qualifier SubModule Registers
(*ePWM[n]).AQCTLA.bit.ZRO = AQ_SET;
(*ePWM[n]).AQCTLA.bit.CAU = AQ_CLEAR;
(*ePWM[n]).AQCTLB.bit.ZRO = AQ_NO_ACTION;
(*ePWM[n]).AQCTLB.bit.CAU = AQ_NO_ACTION;
(*ePWM[n]).AQCTLB.bit.PRD = AQ_NO_ACTION;
//
// Active high complementary PWMs - Set up the deadband
(*ePWM[n]).DBCTL.bit.IN_MODE = DBA_ALL;
(*ePWM[n]).DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
(*ePWM[n]).DBCTL.bit.POLSEL = DB_ACTV_HIC;
(*ePWM[n]).DBRED = 20;
(*ePWM[n]).DBFED = 20;
}
void PWM_ComplPairDB_UpdateDB(int16 n, int16 dbRED, int16 dbFED)
{
(*ePWM[n]).DBRED=dbRED;
(*ePWM[n]).DBFED=dbFED;
}
what could be the issue.