This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280025C: C2000 academy module 5 lab error

Part Number: LAUNCHXL-F280025C
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

Hi Team,

Our customer is learning how to use the LAUNCHXL-F280025Claunchpad and have been going through the c2000 academy. In module 5, he is getting errors when he tried to build the given blank file or the completed example. Also, when trying to open the .syscfg file by double clicking on it brings up the message "Your file was not found, It may have been moved or deleted". What could be the cause of this error?

Regards,

Danilo

  • Hi Danilo,

    Can you please send the full build-error log? The image does not say the full error.

    Thanks & Regards,

    Santosh

  • Hi Santosh,

    Please see attached log file from our customer.

    module5_sysconfig_blinkyled.build.log
    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    **** Build of configuration CPU1_RAM for project module5_sysconfig_blinkyled ****
    "C:\\ti\\ccs1120\\ccs\\utils\\bin\\gmake" -k -j 16 all -O
    Building file: "../c2000.syscfg"
    Invoking: SysConfig
    "" -s "C:/ti/c2000/C2000Ware_4_01_00_00/.metadata/sdk.json" -d "F28002x" -o "syscfg" --package 80QFP --part F28002x_80QFP --compiler ccs
    subdir_rules.mk:9: recipe for target 'build-383871663' failed
    process_begin: CreateProcess(NULL, "" -s C:/ti/c2000/C2000Ware_4_01_00_00/.metadata/sdk.json -d F28002x -o syscfg --package 80QFP --part F28002x_80QFP --compiler ccs, ...) failed.
    make (e=87): The parameter is incorrect.
    gmake: *** [build-383871663] Error 87
    gmake: Target 'all' not remade because of errors.
    **** Build Finished ****
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX
     

    Regards,

    Danilo

  • Hi Dalino,

    Please go to Project Build Settings. Right click on project and select 'Build Setting...', and then go to SysConfig, and delete the entry for "${COM_TI_C2000WARE_SOFTWARE_PACKAGE_SYSCONFIG_MANIFEST}" as shown in the screen below. Press 'Apply & Close' button and rebuild the project. Then, build the project. Let me know if it resolves the issue.

    Thanks & Regards,

    Santosh

  • Hi Santosh,

    According to our customer the same error persists after deleting the entry. Is there other solution to this?

    Regards,

    Danilo

  • Danilo,

    Can you please check what is CCS version they are using? 

    Thanks & Regards,

    Santosh

  • Danilo,

    If they are using CCS 11.0 or older, can they update the latest CCS. The SysConfig compiler may need to be updated which is already part of latest CCS.

    CCS Version 11.1.0 and newer version should work.

    Thanks & Regards,

    Santosh

  • Hi Santosh,

    Here is the response of our customer.

    I am currently running version 11.2. Could this be a problem regarding security settings on my computer set by IT?

    Regards,

    Danilo

  • Danilo,

    I just installed CCS 11.2 and C2000Ware 4.01.00.00 and imported the project and I am able to build without any issue. Can you ask the customer if they see any issue when they import the project? Can you try on your setup?

    Attaching Log below:

    ================

    **** Build of configuration CPU1_RAM for project empty_sysconfig_80qfp ****

    /Applications/ti/ccs1120/ccs/utils/bin/gmake -k -j 3 all -O 

     

    Building file: "../c2000.syscfg"

    Invoking: SysConfig

    "/Applications/ti/ccs1120/ccs/utils/sysconfig_1.12.0/sysconfig_cli.sh" -s "/Applications/ti/c2000/C2000Ware_4_01_00_00/.metadata/sdk.json" -d "F28002x" --script "/Users/sjha/workspace_v11/empty_sysconfig_80qfp/c2000.syscfg" -o "syscfg" --package 80QFP --part F28002x_80QFP --compiler ccs

    Running script...

    Validating...

    Generating Code (c2000.syscfg)...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/board.c...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/board.h...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/pinmux.csv...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/c2000ware_libraries.cmd.genlibs...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/c2000ware_libraries.opt...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/c2000ware_libraries.c...

    Writing /Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg/c2000ware_libraries.h...

    Finished building: "../c2000.syscfg"

     

    Building file: "../empty_sysconfig_main.c"

    Invoking: C2000 Compiler

    "/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --idiv_support=idiv0 --tmu_support=tmu0 -Ooff --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/device" --include_path="/Applications/ti/c2000/C2000Ware_4_01_00_00/driverlib/f28002x/driverlib" --include_path="/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/include" --define=DEBUG --define=RAM --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="empty_sysconfig_main.d_raw" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg" --cmd_file="syscfg/c2000ware_libraries.opt"  "../empty_sysconfig_main.c"

    Finished building: "../empty_sysconfig_main.c"

     

    Building file: "syscfg/c2000ware_libraries.c"

    Invoking: C2000 Compiler

    "/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --idiv_support=idiv0 --tmu_support=tmu0 -Ooff --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/device" --include_path="/Applications/ti/c2000/C2000Ware_4_01_00_00/driverlib/f28002x/driverlib" --include_path="/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/include" --define=DEBUG --define=RAM --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="syscfg/c2000ware_libraries.d_raw" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg" --obj_directory="syscfg" --cmd_file="syscfg/c2000ware_libraries.opt"  "syscfg/c2000ware_libraries.c"

    Finished building: "syscfg/c2000ware_libraries.c"

     

    Building file: "syscfg/board.c"

    Invoking: C2000 Compiler

    "/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --idiv_support=idiv0 --tmu_support=tmu0 -Ooff --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/device" --include_path="/Applications/ti/c2000/C2000Ware_4_01_00_00/driverlib/f28002x/driverlib" --include_path="/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/include" --define=DEBUG --define=RAM --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="syscfg/board.d_raw" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg" --obj_directory="syscfg" --cmd_file="syscfg/c2000ware_libraries.opt"  "syscfg/board.c"

    Finished building: "syscfg/board.c"

     

    Building file: "../device/f28002x_codestartbranch.asm"

    Invoking: C2000 Compiler

    "/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --idiv_support=idiv0 --tmu_support=tmu0 -Ooff --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/device" --include_path="/Applications/ti/c2000/C2000Ware_4_01_00_00/driverlib/f28002x/driverlib" --include_path="/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/include" --define=DEBUG --define=RAM --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="device/f28002x_codestartbranch.d_raw" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg" --obj_directory="device" --cmd_file="syscfg/c2000ware_libraries.opt"  "../device/f28002x_codestartbranch.asm"

    Finished building: "../device/f28002x_codestartbranch.asm"

     

    Building file: "../device/device.c"

    Invoking: C2000 Compiler

    "/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --idiv_support=idiv0 --tmu_support=tmu0 -Ooff --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/device" --include_path="/Applications/ti/c2000/C2000Ware_4_01_00_00/driverlib/f28002x/driverlib" --include_path="/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/include" --define=DEBUG --define=RAM --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="device/device.d_raw" --include_path="/Users/sjha/workspace_v11/empty_sysconfig_80qfp/CPU1_RAM/syscfg" --obj_directory="device" --cmd_file="syscfg/c2000ware_libraries.opt"  "../device/device.c"

    Finished building: "../device/device.c"

     

    Building target: "empty_sysconfig_80qfp.out"

    Invoking: C2000 Linker

    "/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --idiv_support=idiv0 --tmu_support=tmu0 -Ooff --define=DEBUG --define=RAM --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi -z -m"empty_sysconfig_80qfp.map" --heap_size=0x100 --stack_size=0x200 --warn_sections -i"/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/lib" -i"/Applications/ti/ccs1120/ccs/tools/compiler/ti-cgt-c2000_21.6.0.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="empty_sysconfig_80qfp_linkInfo.xml" --entry_point=code_start --rom_model -o "empty_sysconfig_80qfp.out" "./syscfg/board.obj" "./syscfg/c2000ware_libraries.obj" "./empty_sysconfig_main.obj" "./device/device.obj" "./device/f28002x_codestartbranch.obj" "../28002x_generic_ram_lnk.cmd" "/Applications/ti/c2000/C2000Ware_4_01_00_00/driverlib/f28002x/driverlib/ccs/Debug/driverlib.lib"  -llibc.a 

    <Linking>

    Finished building target: "empty_sysconfig_80qfp.out"

     

    **** Build Finished ****

    Thanks & Regards,

    Santosh

  • Hi Santosh,

    According to our customer he suspects that the issue lies in some of their system's security settings. He will reach out to their IT Team to help fix the issue. 

    Thank you very much for your help!

    Regards,

    Danilo