Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: SN65HVD230, C2000WARE
Hi,
1. Is the LaunchXL-F28379D compatible with the 3.3V SN65hvd230 CAN transceiver board?

2. In the datasheet of the LaunchXL-F28379D board, it was mentioned that two CAN ports are available. Out of two, one is visible on the board itself. How can I get access to the other CAN port?

3. This is what I can see on the board. If I have to implement the CAN protocol using this port, how do I connect the pins to the transceiver? Is it done using wires or does the transceiver need to be soldered onto a PCB?
4. Also, if any of the GPIO ports of the board can be used as a CAN port, can I implement the CAN protocol using One LaunchXL-F28379D board and two transceiver boards?
Thank you
Karthikeya